Part Number: ADS8681
Other Parts Discussed in Thread: ADS9226
Hi team,
If I have a differential output signal (voltage sensing from the AMC33x), and since this device has a single-ended input, how can I make use of the full dynamic range instead of only using half the voltage of the AMC33x? Do I have to use a differential input device like ADS9226? If so will the "pseudo-differential" input work and what is the difference between pseudo-differential and differential?
Thanks,
Lauren