Part Number: TSW1400EVM
Other Parts Discussed in Thread: DAC5681EVM
Myself and my lab group are interested in purchasing the TSW1400EVM and interfacing it with the DAC5681EVM.
We have some specifications, and I am wondering if the combination of these devices can accomplish our goals:
- Generating arbitrary waveforms of 10 microseconds long at 1 Gsps.
- +/- 1V amplitude with computer control
- Generation of sine waves that can sweep from 100MHz to 200MHz
- Triggering rate of 100kHz
- Record Length of 10,000 samples
- What is the update time?
- Are both devices needed or can we send a waveform directly to the DAC5681EVM from a computer without the TSW1400EVM?