This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dear,
The customer uses TVL5630, with two output channels connected in parallel and set as dual complementary outputs, but the temperature range can only support -40 to 85. Is there a compatible model that can support up to 125?
Hello Anna,
We have a much better device but unfortunately it is only 4 channels - DAC43204. The device has a slew rate control, high-Z output for voltage margining, appropriate temperature range, force-sense control capability, and NVM to store configurations.
If 8-ch is required, DAC43508 would be another good device, but it will not have an option of adjustable slew rate control.
Thank you,
Illia Volkov