I am working with the AFE10004EVM board and software to read a remote temperature sensor but am running into a few issues with what I think is the software but could be the hardware. When I'm in the software and try to switch over the sensor for DAC drop down to remote but it will not let me save or enable the LUT without switching back to the local temp. Is there anything specific I need to do for setup to allow the remote sense to be selected? Also, could there be something I hooked up or jumped incorrectly on the board that would be not allowing this to be selected?