Part Number: AMC1333M10
Other Parts Discussed in Thread: AMC3336
1. Have to measure 1000Vdc in isolated.
2. Is there any example c code for AMC1333M10 , to interface with MCU?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AMC1333M10
Other Parts Discussed in Thread: AMC3336
1. Have to measure 1000Vdc in isolated.
2. Is there any example c code for AMC1333M10 , to interface with MCU?
Hi Deepak,
Thank you for your question!
Best regards,
Samiha
Hi Samiha,
1. Can it be interfaced on SPI or uart interface with MCU?
2. Have to measure 1000Vdc & 300A via shunt resistor
a) For voltage sensing , found that https://www.ti.com/product/AMC3336 has inbuilt dc-dc also, so simplifies design, so can use it
b) for current sesing found https://www.ti.com/product/AMC3306M05 , also has inuilt dc dc
will these 2 be ok for design in 1000V/300A application?
Hi Deepak,
Thank you for your patience.
I hope that helps!
Best,
Samiha