Part Number: DAC81402
Hello everyone,
I seek assistance properly designing the electrical overstress protection circuit for my DAC81402.
Following the EOS protection scheme shown in its datasheet, I choose the TVS D3 with a Vclamp=67V, the ferrite bead FB1 with a 120Ω @100MHz, the diodes D1 and D2 have a forward voltage Vf=0.7mV.
How high should R1-R2 (and R3) be to sustain ESD pulses? For example, I can consider an 8 kV IEC ESD (contact discharge).
In the datasheet it is assumed a R1=10Ω, how has it been chosen? Would it be enough for this application?
Thank you,
Davide Tosatto