Other Parts Discussed in Thread: ADS9218
Hi Gent.,I have one quesiton.. on ADS9120, could you please help check it? thanks.
In the d/s, this can support 2.5MSPS sample rate, I want to know what the maximum input signal bandwidth is? Based on Nyqusit law, the maximum input signal freq. is 1.25MHz, but in d/s, it has no relative description on the input signal bandwdith limitation. Also the electrial char. spec., when Fin is 500KHz, the SNR only is 84dB. As we can see as well, when the input signal is 100KHz, it can get much better ADC SNR perforamnce. I'm curious of that when the input signal is 1MHz, if ADS9120 can support it? how about the SNR spec. at this condition? In my system, the Fin is 1000KHz, I only can get ~70dB SNR spec., I want to confirm this is chip limitation or my system design limitation? thanks.
Have a good day!
Jay