This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J58EVM: FPGA load fails

Part Number: TSW14J58EVM
Other Parts Discussed in Thread: ADC12DJ5200RF

I today did receive a replacement card:
Label: " TSW14J58EVM DC182_A8"
There is no indication whether Rev A or C aka 5.5V or 12V power supply to be provided.
S/N 7944400011

Please assist.



Hi experts,

I was running TSW14J58EVM

REV A  FT6DN1XZ-TSW14J58

for just a while,

but first the GUI was no more able to load JMODE images via mini USB
(WIN10 device manager did show error). I then did work around loading FPGA with JTAG debug port
directly. Second unfortunatelly also XILINX hardware manager can not auto connect to board any more
since last week.

Note: USB3  port is running quite well, but this cannot load FW.

Question: are there other know problem loading via USB/ JTAG with Rev A?
                 I got a hint from german support, but connection is still failing 
                 either 5.5V 5 A as well as for 6V 4A supply provided.

              ---------------------------
             Was the current on the power supply turned down by accident or did they change the power supply?
             Typically we find customers using a lower current than necessary to load/program the FPGA.
             Please make sure the customer have 4A for the 6V, J58 power supply.
             ---------------------------

 Question: TSW14J58EVM is listed not available at Mouser/ Digikey.
                 Is there still a replacement or successor for J58?

Regards

Roland