Part Number: DAC70004
Hi there,
Do these devices have internal clamp diodes on the output? I do not expect output currents of more than 10mA from the DAC and so this may be sufficient if there are internal clamp diodes to prevent the output swinging beyond +0.3V VDD and -0.3V GND (e.g under ESD condition). Do I need to add these diodes externally?
Many thanks.