Part Number: ADS5400
Hi,

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS5400
Hi,

Hi KJ,
No, this is not valid. This is a periodic RESET signal. In the current configuration, your RESET is latched on two sequential falling edges of the clock. This will result in two sequential SYNCOUT pulses repeating every 4 samples.
To achieve what you are asking for, RESET should only be high for one clock transition and then low for 3 as in the below image. This will result in the SYNCOUT occuring every 4th sample.

Be sure to note the 7 CLK latency of N is the same as the latency between SYNCOUT and the latched RESET.

Regards, Chase
Hi Chase,
thank you for the answer,
1) regarding only CLKOUT dividers, will waveform in my original post correctly align them between multiple ADS5400s?
(Assuming I'm ok with SYNCOUT for multiple times, when RESET is latched in high state,
but will CLKOUT stay in the same phase for all parts after the first RESET period and initial alignment).
2) Or maybe RESET=CLKIN/2 is a better idea to just align the dividers?
Best regards
Hi KJ,
If you are only wanting to align the data once after power up, any width pulse is sufficient. The periodic signal is just to maintain that the phases are aligned throughout data capture. Any CLKOUT/N where N is an even integer should be sufficient and allow the timing to workout. CLKOUT/2 or CLKOUT/4 will be fine.
Regards, Chase