Other Parts Discussed in Thread: INA128, PGA308, MSP430F5659, INA851, ADS8168, ADS8860, OPA320, PGA309, INA849
I am designing a load cell amplifier. The load cell output/amplifier input is 2mv/v, and the amplifier's output is 3V. I need an A/D's sampling speed to be 200k-500k.
Would the INA128 be OK? if not please recommend a better amplifier and A/D. Currently I'm using a PGA308 for the amplifier, and the MSP430F5659's built in 12Bit A/D for the A/D, but the repeatability is too low, varying by +/-3-4 LSB. I believe a more precise A/D, such as a 16bit one, will contribute to better repeatability, as well as a faster amplifier.