1) power up device (I am using the EVM card without the USB host - the host won't recognize the eval software. Pulled all the host related jumpers)
2) try to unlock chip and set to 4 wire SPI. It does not seem like the chip even notices SPI.
I have had it working for hours on 4-wire writing and reading channels but then it stops recognizing SPI. That was with loose wires everywhere. Now that I have everything cleaned up and firmly attached it won't go again. I think somehow I got it to start again but only by some bad random SPI transfer? I have tried 2 EVM eval boards.
Here is what I think is needed (below), As read back by a SPI monitor. Like I said, I did get it into 4 wire mode twice, and used SPI reliably for many hours, but a power cycle hosed it.
And how does the chip "automatically" detect the SPI protocol? I have tried clock rates from 1.25M to 312.5K Hz
I am at wits end.... thanks for any help.
Here is an example waveform: