Good day,TI expert.
I'm DDC264 new user ,so I was confused when I saw the Analog input to AGND in 7.1 Absolute Maximum Ratings(the maximum voltage just 0.7V !!!).
So I want to be sure the maximum voltage of analog inputs is 0.7V or 6V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Good day,TI expert.
I'm DDC264 new user ,so I was confused when I saw the Analog input to AGND in 7.1 Absolute Maximum Ratings(the maximum voltage just 0.7V !!!).
So I want to be sure the maximum voltage of analog inputs is 0.7V or 6V.
Hi,
AVDD is for power supply pin, which is shown in the 2nd row of the pin functions table you showed.
Analog input is for those input pins for analog signal inputs.
Thanks