This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC81408EVM: output always 0v

Part Number: DAC81408EVM
Other Parts Discussed in Thread: USB2ANY, DAC81408

Hello  Team

I'm trying to control the DAV81408EVM with USB2ANY interface adapter and GUI from DAC81408EVM software downloaded for the TI website.

I use internal 2.5 V reference, Supplying the board with VDD/VAA = 5 V, VCC = 12 V VSS = -12 V and VIO = 3.3V (supplied from the USB2ANY adapter)

1. the jumper settings are follows.

Jumper

Default Position

J2

Open: /RESET deactivated

 

J3

Open: /CLR deactivated

 

J9

Closed: GND

 

J10

1-2: USB2ANY 3.3V on J8.5

 

J11

1-2: VREF from REF5025

 

J12

2-3: VSS on J7.2

 

2. DEVICE_ID  reads value 0X0A60.

2.STATUS   reads value  0x0008.

3.SPICONFIG reads value 0x0A84.

in DAC81408 page, changed DACOUT,  its always seems zero.