Part Number: ADC32RF42
Hi,
I have 2 questions, First one is a general question not exactly related with the part and I'd appreciate if you can give an answer. Since sysref frequency is way smaller than the device frequency of an FPGA or ADC32RF42, why do we care about setup and hold time violations? Doesn't device clk rising edges sample sysref signal many times(since sysref signal is way slower than sampling clocks) when sysref is high?
Second question is related with the part ADC32RF42. On page 46 of the datasheet, table 14 shows the data alignment when the adc is used in 12 bit bypass mode. It looks like no data is sent through lanes 2 and 3 according to table 14. Is this correct? If so then will I need 1.5Gs/s x (64/5)x(10/8)=24Gb/s interface? Since only 2 lanes are active(according to table 14) I need a lane rate of 12Gb/s which means I can not use a kintex 7 FPGA . Am I correct? Can you please enligthen me..