This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1015: How to define the formula to measure the voltage

Part Number: ADS1015

Hi TI expert

Could you pls help to explain how to define the formula to measure the voltage input on ADC channel.

Add more information: we want to measure one voltage with upper limit is 3.3V connect with AIN0, then which FSR shall we choose? is +-4.096? 

Is the formula correct? voltage = 4.096* adc / (0.193* 4095), 0.193 is the factor of input voltage, 4095 is the Dec value for 12bits.

Thank you!

BR

Weicheng