Other Parts Discussed in Thread: ADS114S08
I am using ADS114S08 evaluation module. I am currently analyzing the temperature sensors compatibility of the board and using a Pt100 sensor. When running the script of 4 wire rtd at room temperature, the voltage is 0.28V approx. When i am measuring the voltage across R68, it is 1V. I am not sure what 0.28V means
To further clarify, I am getting 0.28V on the delta-sigma software after running the 4 wire rtd script (measurement image attached). I am not sure what is this measurement conveying? As in, what is 0.28V?
What I expect is, the rtd and r68 are in series, where rtd is connected to avdd and r68 is connected avss, adc is connected across r68 and rtd is connected to avss. What i was expecting was tht voltage across r68 will be the output of adc and power supply - voltage across r68 will be the voltage across 68. voltage across rtd divided by excitation current (1mA) will give the resistance of rtd and then from the lookup table, temperature could be checked. But its this 0.28V which was unexpected.