Part Number: ADS1258
I've been working on a project using the ADS1258, and I have two different ICs on two different boards with different part markings. On one board, the label on the IC has the TI logo and the IC on a completely different board does not have the logo. I'm just trying to help confirm that the second IC without the logo is legitimate. 99.9% sure it probably is, but just curious if anyone has insight. Could be something as simple as the parts were made in different fabs with different capabilities for labeling. Of course for my purposes, the one with the logo is the board I'm not having troubles with, while the other non-logo part I'm having issues with. Most likely user error on my part, but I'm looking to cover the bases. The one with the logo was sourced from an authorized distributor, and at this time I'm not sure of the provenance of the second IC. Hopefully the images come through below.
Thanks!