This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS114S08: Is it possible to use ADS114S08 instead of ADS114S06 with same software

Part Number: ADS114S08
Other Parts Discussed in Thread: ADS114S06,

Dear Specialists,

My customer is considering ADS114S08 as substitute for ADS114S06.

These are pin compatible.

At the point of control signal, it is possible to use the same control signal ?

I appreciate your great help in advance.

Best regards,

Shinichi

  • Hi Shinichi,

    The ADS114S08 is the extended function version of the ADS114S06 and can be used as a direct replacement without the need for code changes.  The difference relates to the number of possible analog inputs for the S08 version.  Both the S06 and S08 can be used for GPIO control in the same manner of control.

    Best regards,

    Bob B

  • Hi Bob,

    Thank you for your quick reply.

    I understand that the software for the ADS114S06 can be used for the ADS11S08 as well.

    I think the customer concerns will be resolved.

    I appreciate your great help and cooperation.

    Best regards,

    Shinichi