This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7552: No output from the DAC7552 channels.

Part Number: DAC7552


Hi,

I'm doing a PCB design using DAC7552 and I've designed the PCB according to the following schematic design. Is this correct?  

I'm not getting any output from the DAC channels, I didn't use any power down command and directly used the following command in a 16bit data frame through SPI communication.

Power down commands in the datasheet are really confusing, as there are multiple occurrences for the same scenario. 

Am I missing something here?