Other Parts Discussed in Thread: ADS5263EVM
Dear Sir or Madam,
Will the FMC-ADC-ADAPTER work with the ADS5263-EVM? The ADC is not listed on the flyer of the FMC-ADC-ADAPTER.
Best Regards,
Uros
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir or Madam,
Will the FMC-ADC-ADAPTER work with the ADS5263-EVM? The ADC is not listed on the flyer of the FMC-ADC-ADAPTER.
Best Regards,
Uros
Hi Uros,
You are correct. Unfortunately the SPI interface was not routed on the ADS5263EVM to go to this connector directly, so the USB of the EVM will need to be used unless you can connect available GPIO of the ZCU102 to the following test points on the ADC EVM. Since this device supports 1.8V CMOS and 3.3V CMOS digital IO levels, if your FPGA is using 1.8V CMOS logic for this GPIO then this should work smoothly.
Thanks, Chase