Other Parts Discussed in Thread: ADS8668
Dear team,
My customer is using ADS8688 as V/I measurement in PLC application. When they plan to expand the scale range of the input using below circuit. they measured the AIN_5P and AIN_5GND with 2.2V and 1.2V value although there is no input on the AIN_5. Is it because of the floating of AIN_5 cause this happen? Since if AIN_5 input 0V , it is normal 0.