Part Number: ADS1293
Hi team,
Can you have a look at the following customer inquiry, please?
We are currently working on a project in which we would like to incorporate the ADS1293.
I have two questions:
1) OpenLead
We want to use the ADS1293 in a pure 3-Lead/3-Channel (without feedback -RLD) configuration:
This works fine so far.
Now we have a problem with the OpenLead detection. According to the datasheet neither the DC- nor the AC- detection of the ADS1293 would work (because no RLD). Only the variant by means of impressing AC voltage and subsequent analysis (FFT/narrowband filter) would work. But this would cost a lot of energy which we don't want to spend (or can't).
Do you have another solution as a suggestion?
Is it possible to use the DC version by connecting the RLD internally?
2) Reference pin (CVREF):
We would like to use the voltage at the reference pin (CVREF) for other purposes.
Actually the datasheet is very clear here ("The CVREF pin must have a 1 μF bypass capacitor-to-ground with low ESR and is not designed to be loaded with other circuitry.").
Is it still possible to decouple the voltage via a high impedance converter?
Thank you,
Franz