Part Number: ADS124S06
9.3.8 Bias Voltage Generation 図76. VBAIS Block Diagramについて分割抵抗がR, 5R, 6R と記述されています。
R 1つの定数の数値をご教示願います。可能であれば、R の許容差および温度特性も含めてご教示頂けると幸いです。
2023/7/14 まで一報いただけると幸いです。
以上、お手数おかけしますがよろしくお願い致します。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS124S06
9.3.8 Bias Voltage Generation 図76. VBAIS Block Diagramについて分割抵抗がR, 5R, 6R と記述されています。
R 1つの定数の数値をご教示願います。可能であれば、R の許容差および温度特性も含めてご教示頂けると幸いです。
2023/7/14 まで一報いただけると幸いです。
以上、お手数おかけしますがよろしくお願い致します。
Hi Masamitsu Hayashi,
Welcome to the E2E forum! E2E is an English language forum only, so please translate prior to posting. The bias voltage is a simple voltage divider. It is meant not as a precision source but rather a simple bias voltage to place sensors, such as a thermocouple, into the correct measurement input range for the ADC. The voltage output from the resistor divider is buffered, but the buffer has a relatively large output impedance (350 Ω typical at room temperature). So the buffer cannot drive a lot of current without affecting the bias voltage at the device pin.
Generally silicon resistors are not that precise but are well matched within a process. The precise value of R was not given from the design team, nor was the tolerance. The term 'R' is there to give you an idea of how the bias voltage is created. Also note that the bias voltage is between AVDD and AVSS. If you need a precise bias voltage with a low output impedance, then you should use an external bias voltage source.
Best regards,
Bob B