Hello,
I'm working on a synchronisation of two TI DACs with a module generator pattern TSW3100 and i have few questions:
I have choose the TSW3100comm_signal_pattern to generate an WCDMA-TM1 signal, on the TSW3100 control panel:
- The TSW3100 includes the ability to synchronize multiple boards using a master/slave synchronization, witch mode should i use for the best results and why?
- with LVDS mode the data are always interleaved, but the connection between FPGA and DAC348x provides 16 LVDS differential data bits, is it necessary to choose this mode if the connection is allready done?
on the software DAC348x_GUI_V3p3, in input format panel how can i choose between Input data: 16bit single mode or 8 bit dual mode? how and why i choose one or another?