Hi,
I am struggling a bit with the ADS8689 A/D converter. I get a readout that makes sense with the default range setting. Attempting to switch to range mode 0x0B (1.25 × Vref) doesn't change the readout.
Will someone please confirm (or disconfirm) that the SPI command needed to switch the range selector to 0x0B, while keeping the internal reference enabled, is the following set of bytes?
[0xD0] [0x14] [0x00] [0x0B] (in that order).
As I understand the datasheet, this means:
- [0xD0] Write 16-bit word
- [0x14] Range select register
- [0x00] Data byte for 8-bit register 0x15 (reserved)
- [0x0B] Data byte for range select register
Any help will be greatly appreciated.