Part Number: DAC63204
Other Parts Discussed in Thread: DAC63004,
Hello,
Can the DAC63204RTER and DAC63004RTER be used interchangeably without modifying firmware, or are there functional differences between the two that prevent this?
Thank you,
Kyle
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kyle,
Yes, they can be used interchangeably. There are no changes that need to be made if you are going from the DAC63204 to the DAC63004. If you were going from the DAC63004 to the DAC63204 then the only feature you would not be able to use is the deep sleep power down mode.
Best,
Katlynne