Part Number: ADS124S08EVM
On Windows 10, installed "DELTASIGMAEVAL-GUI-installed.exe", "ADS124S08-dvcpkg.exe" and confirmed that ".Net Framework 4.5" or higher has been installed but still unable to connect to hardware.
Thanks,
Ben

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS124S08EVM
On Windows 10, installed "DELTASIGMAEVAL-GUI-installed.exe", "ADS124S08-dvcpkg.exe" and confirmed that ".Net Framework 4.5" or higher has been installed but still unable to connect to hardware.
Thanks,
Ben

Hi Benjamin,
Yes, you have a driver issue. The driver itself is a basic MS-OS driver, but may not correctly associate if the driver file was not installed correctly before the EVM was plugged into the USB. See if this thread can help get you going:
Best regards,
Bob B
Hello Bob!
Thank you! That fixed it. My only comment is that this information would be very useful in the otherwise very well documented TI User Manual.
Thanks,
Ben