Hi,
I am accessing the ADC128S102 over a SPI interface. When I look at the DOUT line, it doesn't seem to make sense to me (see photo).
The device is running off 3.3V. I see a 3.3V pulse but it is happening when 0s are supposed to be outputted from the device. After that the output goes down to approx 1.8V.
Other than replacing the device I am wondering if there is something that I may be doing wrong?
Clock is in yellow. DOUT is in purple
Thanks,
Jeff