I am doing a detailed tolerance calculation for an interface, which is measured with this ADC.
- Are the 2 channel-to-channel matching errors (gain and offset) reflecting the fact, that for example if the gain error of let’s say channel 1 is at 96 LSB, then for any other channel it will not be more than 60 LSB difference to channel 1?
In my example each other channel would be at > 36 LSB? - In the table of chapter 6.5 (electrical Characteristics), the section “EXTERNAL REFERENCE INPUT (REFSEL=0)” there is a Parameter “VREFIO_EXT” mentioned with typ, min, max value.
In my opinion, this is a recommended operating condition regarding an external used reference. I don’t think it reflects the reference voltage range, where the other performances (especially Gain error) are in their given range. This range is much higher than the internal reference range. - I don’t find an information, on how the reference voltage influences the conversation result. The accuracy of the external reference can have a significant influence on the accuracy performance of the ADC. The Section “7.3.9 ADC Transfer Function” don’t even mention the word reference.
In my opinion, if I have a full scale range of 10 V (+/-5V Range selected), a deviation of the reference voltage nominal value of 2.5V will have an impact of 4 times the deviation. Or am I wrong?