Other Parts Discussed in Thread: ADS1298, INA333
Before asked as to why i'm using ADS1298 instead of 99 for EEG, it's cuz the latter is out of stock and i'm working with what I have at the moment.
I understand that the noise floor is high so, i'm using a differential instrumentation amplifier (ina333) - electrode and a reference electrode. Even though I said differential, it's how the electrodes are recorded by through the instru. amp the input to the ads1298 is single ended.
My battery is 3.3V and i have a 1.65 voltage reference, the ina333 REF pin is tied to the 1.65V as i'm using only a single supply.
Concern 1
In the ads12988 datasheet and through other questions on here I understand that if AVDD is 3.3v and AVSS (the analog ground) = 0V and my mid supply voltage is 1.65V. Where do I connect the mid supply voltage on the chip?
What about Vref, there is VREFP and VREFN on the chip, how to select the value for those? Is it just set to mid supply? It seems like the VRef value dictates the input voltage range of the ADC, can anyone please shed more light on this?
Can I leave the Dgnd and Dvdd unconnected if i'm supplying the digital side straight from my battery, I don't see the need to use the ads1298 as the digital supply, just an additional step, any problems that might arise?
Concern 2
It looks like the RLD on the ads1298, bias's the body to mid supply rather than doing it based on the common mode, would anything happen if I used the ina333's common mode for the RLD with an external opamp to inject this voltage instead of the RLD pins on the chip. Hence leaving the pins unconnected (RLDINV, REF, IN, OUT)
Concern 3
Do i even need a ina333, although many sources highlighted the need. The output of ina333 will be centered around 1.65 with the signal amplified n amount, that supposedly solves the concern of the noise floor right? But I can see how there should be another way to just center the input around a reference on the chip itself. Once the signal is centered around dc level, is any gain even required? How to calculate gain need on ADS1298 and ina333 (if needed).
I'm concerned that using a high enough gain for the pre-amplifier, if needed, defeats the purpose of a 24bit ADC, just unsure how to calculate as such.
Any help would be much appreciated