hi sir
I want to search a solution ,better than AD7766
Did you have any advise?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi sir
I want to search a solution ,better than AD7766
Did you have any advise?
thanks
Hello Chen,
Yes, the ADS127L21 is a good option verses the AD7766. The ADS127L21 is a delta-sigma topology where the AD7766 is an oversampling SAR.
The ADS127L21 has a wide range of filter options, including wideband (brickwall) filter and low latency SINC filters.
A few of the key specifications:
Wide dynamic range (SINC4 filter, MAX speed mode)
110.9dB dynamic range at 512ksps
123.3dB dynamic range at 32ksps
Low Power
14mW at 200ksps
4.3mW at 50ksps
High DC accuracy
INL: 0.4 ppm of FS (typical)
Offset drift: 50 nV/°C (typical)
Gain drift: 0.5 ppm/°C (typical)
Regards,
Keith Nicholas
Precision ADC Applications