Other Parts Discussed in Thread: ADS131M04
Looking for review of an ADC part selection - ADS131M04. Our application has a fully differential OpAmp driving a 6" mico-coax cable. The Diff Amp is powered with +/-2.5V and has a single ended input of 0 to 2.5V. This should result in an AINxP signal of 0 to +1.25 and an AINxN signal of 0 to -1.25V.
Our questions,
1) We are considering offsetting the Diff amp so the single ended range is -approximately -1 to +1 V to the Diff Amp input. In this case the Diff output voltage to the ADC will be +/500mV on each input (AINxP ,AINxN ). The question is does the AINxN input accept negative voltages from a differential amp? Some of the ADC in the series do not. It appears that it does, but a similar part (ADS121B04) states the min analog input as AGND - 0.1.
2) Does this type of ADC (sigma delta) require any local buffering to avoid kick-back or other signal data acquisition errors.
3) Can the part be clocked such that the output rate is ~10kHz? For example, if the OSR is 256 the clock would be 5.12MHz.
3) Given that there are (4) ADCs that are simultaneous, it is assumed that the stated sample rates at the different clock rates and OSR values are for all 4 channels. For example, Clock = 8.192MHz, OSR = 256, the sample rate for all 4 channels is 8Ksps.
Thank
Rob.