Part Number: ADS124S08EVM
Other Parts Discussed in Thread: ADS124S08
Hallo,
What is the best configuation to read the internal temperature sensor and the best way to convert the value to °C?
1. Is it better to use VREF = 2.5 V than VREF = AVDD? Is it possible to acquire a channel using AVDD as VREF (ratiometric) and then switch to 2.5 V to read the internal temperature sensor?
2. From the datasheet: Output Voltage = 129 mV @ Ta = 25 °C
Temperature coefficient = 403 uV/°C
Output Voltage = m * Ta + n
Ta = ( Output Voltage - n ) / m
with:
n = 129E-3 - 25 * 403E-6 = 118,925E-3 V
m = Temperature coeff. = 403E-6 V/°C
Thank you
Matteo