Part Number: ADS5295EVM
Other Parts Discussed in Thread: ADS5295
The ADC board was made by referring to the circuit diagram of ADS5295EVM.
When I applied 50MHz Single Ended Clock to ADS5295, 50MHz Clock was observed on LVDS P/N Pin at ADC Clock Out.
Then, I tried to read the register by writing 0x0001 to the internal register address 0x01 of the ADC according to the timing chart shown in the ADS5295 Datasheet, but the data returned was all zero.
The SDOUT Pin of the ADC also seems to be tied to 0V.
If I write 0x0000 to Address 0x01, the SDOUT floats, so the ADC seems to recognize the serial command.
I would appreciate any suggestions on what I should check.