Part Number: ADC12DJ1600-Q1
Other Parts Discussed in Thread: HD3SS3411-Q1, HD3SS3411
Team,
Customer is trying to validate the ADC12DJ1600-Q1 and in order to do that theyalso have to measure the switching time for the MUX.
Below is a screenshot of the oscilloscope where:
- Yellow - SEL signal
- Green - Port A
- Blue - Port B
- Purple - Port C

Two questions regarding this topic:
First will be at what percentage of the signal do we have to measure this? 80%?
And the second one is it: do we have to measure the time until the signal B becomes high? So the second cursor (the one with a dotted line) should be a little to the left? So the time would be below the limit of 1ns (right now it is at 1.64ns).