Other Parts Discussed in Thread: TSW14J57EVM
I hope this email finds you well. We have a question regarding the HSDC Pro GUI and the Capture Option as mentioned in the datasheet (slwu087e.pdf) under section 3.1.3.1.
According to the datasheet, it is mentioned that for the TSW1400, which has 1GB of RAM and a 4-channel ADC, the maximum number of samples per channel that would use all memory is 131072 Msamples. Similarly, the TSW14J56 with 2GB (32Gb) of RAM allows up to 2,147,483,648 16-bit samples divided by the number of channels. The TSW14J57 has 1GB (16Gb) of RAM, which allows up to 1,073,741,824 16-bit samples divided by the number of channels. The TSW14J58/59 with 1.5GB of RAM allows up to 1,610,612,736 16-bit samples divided by the number of channels. These sample amounts are calculated under the assumption that no tail bits are present in the data frames.
Based on this information, it seems that the TSW14J57 can capture up to 1G samples. However, we are interested in capturing 2.5G samples. Is it possible to configure the TSW14J57 to achieve this?
Any assistance or insights you could provide on this matter would be greatly appreciated.
Thank you for your time and support.
Best regards,