Hi Team,
What are the expected voltage levels when the TMSTP_LVPECL_EN is set to '1' ?
Can you tell me how the voltages of LVPECL fit with the requirement for common mode
please refer to section 6.3 - Recommended Operation Condition.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
What are the expected voltage levels when the TMSTP_LVPECL_EN is set to '1' ?
Can you tell me how the voltages of LVPECL fit with the requirement for common mode
please refer to section 6.3 - Recommended Operation Condition.
Thanks
Hi Ohad,
LVPECL here is bit of a misnomer. The common mode requirement when setting TMSTP_LVPECL_EN is set to '1' is as shown below.

Each diff leg for TMSTP is connected to ground with 50 ohms.

Regards,
Neeraj