Part Number: ADS1261EVM
hi everyone:
We are using the ads1261EVM evaluation board for functional evaluation, which needs to use the external trigger single acquisition mode. We have checked all the ways to use the evaluation software, but there is no way to know how to configure it.
At present, the script configuration of holdstart 1 can basically synchronize the start pin signal with the drdy signal at one shot mode, but when the collect command is used to collect data, it will cause stalling. It should be because the method of obtaining data is still to send the start command via spi when this command is used. Is there a way to turn off sending the start command via spi? In addition, using the rddata command can read the adc data once, but cannot read continuously to acquire the signal