Hello,
I am using ADS1299 with Bipolar supply voltages (+2.5V , -2.5V) and internal reference (4.5V) with 250 SPS. I want to give a signal from function generator and get the same signal at the output.
I am giving 10mVp-p signal from Function generator as input. Below is the connection setup,

The data logged is in microvolts amplitude.
Below is the logged data for gain = 1, (5000 samples). X -axis = Sample number, Y-axis = microvolt (uV)

Below is the logged data for gain = 24, (2000 samples). X -axis = Sample number, Y-axis = microvolt (uV)

Could you suggest if I am missing any settings? Why am I not able to produce the same sine wave of 10mVp-p at output? Please suggest what should I do.
Thank you,
V. Vedashree