This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3660EVM: How to confirm the value written to ADC register

Part Number: ADC3660EVM

Hi,

I am using a linux utility "spidev_test" to write into ADC register.

For example if I want to write a value of 0x6c  at offset of 0x70 , I use the following command:-
$ spidev_test -D /dev/spidev1.0 -s 1000000 -H -O -b 8 -S 1 -p "\x00\x07\x6c"
(This command loads the bitmapper)


Now how can I confirm that the value is being written at offset 0x07? 
Is there any other linux utility using which I can achieve this?


If possible please suggest me a easy way(Linux based) using which I can read and write into these registers

Thanks,
Sameeksh M Shetty