Part Number: ADS5409EVM
Other Parts Discussed in Thread: CDCE62005EVM, CDCM9102, CDCE62005
Hello,
I have purchased the ADS5409EVM and TSW1400EVM kits. I have connected these kits to each other using the relevant interface points. After that, I am supplying power to both the ADC and the Capture Card via USB. Additionally, I am providing 5V power to the Capture Card's power input. However, I am encountering an error (DDR Error, Time out) while capturing data using the HSDC Pro application. Moreover, the USER_LED3 is not lighting up. Could this be due to not supplying a clock to the ADC card? Do I need to provide an external clock to the ADC card? If I need to provide an external clock, what should be the frequency of the clock in MHz to achieve a sampling rate of 900 MSPS? I would like to use the device up to a sampling rate of 900 MSPS.
Thank you.