does ADS8326IBDRBR, SON-8 fit 1:1 on the solder pad layout of ADS8326IBDGKR, MSOP-8 fit on the same solder pad layout?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
does ADS8326IBDRBR, SON-8 fit 1:1 on the solder pad layout of ADS8326IBDGKR, MSOP-8 fit on the same solder pad layout?
the MSOP-8 from the datasheet is now called VSSOP-8, right?
Hello Hanno,
Thank you for your post.
Yes, VSSOP is the same as MSOP-8.
The package outlines and the land pattern data for both packages are available at the end of the ADS8326 data sheet. The DGK package has a body width of 3 mm, while the total package width for the MSOP-8 package is 3 mm.


Regards,
Ryan