Whether the ADS7138 has an interrupt function. The customer wanted to use an ADC to collect 5V for monitoring. 12-bit, IIC interface, no rate required, whether 7138 can be used. Or is there any other recommendation
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Whether the ADS7138 has an interrupt function. The customer wanted to use an ADC to collect 5V for monitoring. 12-bit, IIC interface, no rate required, whether 7138 can be used. Or is there any other recommendation
Hi aiwen,
The ADS7138 has an 'Alert' output which could be used as an interrupt to the controller. It has programmable thresholds as well as some built in noise filtering capabilities.
Hi tom;
I am very appreciate to receive your response,I would like to check again whether it can be used to collect 5V voltage?Thanks!
The ADS7138 uses AVdd for its reference. With a 5.1 to 5.5V supply, you can monitor a 5V input. With a 5.0V supply, you could use a voltage divider on the 5V source that you plan to monitor.