This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC8565: Analog Output, Package-Package Time Skew

Part Number: DAC8565

Hi there!

Multiple DAC8565s are used in a project. The settling time is given 8us (typ) and 10 us (max) in the datasheet. My question is about the variation of this parameter between multiple DACs operating at the same temperature. Assuming that digital interfaces are perfectly synced, what would be the expected synchronicity between analog outputs? Let's say that DAC1 has 8 uS settling time. Can DAC2 (at the same temperature) have 10 uS settling time? Can we estimate the expected synchronization error on analog outputs between DACs operating at the same temperature?

Thank you.

Alper