Part Number: ADS131E04
Good afternoon everyone,
I am needing help regarding this IC, even though it is mainly for power measuremenet i want to read 4 load cells simultaneously.
The load cells are connected to 5V, they have a sensitivity of 2mv/V so at 5V it would give a 10mV.
ADS131E04 VREFP and VREFN are connected to 5V and AVSS respectively.
Eveything works fine, communication is fine, read and write register is also fine.
The issue is that i always get values around 0xFFFA00 even short circuiting any differential input pair (for example channel 0 IN0P and IN0N). Doing so, i should be getting a reading of around 0 but i get also 0xFFFA00 +- 10 (always moving but in +-10 counts)
What could be the issue? this thing is driving me crazy...
Best regards
Eduardo