A couple of questions here on behalf of an assigned customer:
1. The Abs Max ratings for the AIN_nGND pin is +/-0.3V. I assume beyond this level the ESD structure is activated. If the current into/out of the pin is externally limited, what is the max current the pin can tolerate w/o damaging the device? I would assuming something in to few mA range?
2. If AIN_nGND exceeds the +/-0.1V recommended limit, but is less than the +/-0.3V abs max for these pins, do we expect a shift out output code from the ADC? Understand that this is out of bounds of operation, just wanting an idea of what to expect from the ADC for possible software error checking, etc...
Thanks!
-Steve