Part Number: AFE58JD48EVM
Hi, we have 2 questions about the EVM:
1) We are using the EVM board's GUI to configure the ADC chip, and for initial testing, we also use the internal ramp generator( default setting for its data format ) to test the LVDS I/F going to an FPGA EVM. The datasheet doesn't mention the data format of the generator. Is it unsigned or 2s complement ? If the output format can be configured, we'd like to know how.
2) Once all GUI configuration steps are done, we want to change the clock from using 40MHz ( confirmed ) to prescale it down to 20 MHz. Is the prescaler in register 0x29 and are there any other registers to be changed to make the new setting take effect ?