This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5832LP: The number of samples of swaroop boards using TX7332 and AFE5832 cannot be changed

Part Number: AFE5832LP

We want to use SWAROOP to achieve some ultrasound applications, but 50MHz-2030 sampling points can only achieve a few US acquisition. For other AFE boards, I see that the number of sampling points in their GUI can reach 65536, why can't I set it here

  • Hi,

    Swaroop board uses very low end FPGA to meet lower cost and lower power. With the given memory in the FPGA, we could capture this much samples only. If you want to capture more samples then you can use delay feature give on main page. So in first time you capture the N samples then apply delay equivalent to N samples and capture again for next N samples. 

    Regards,

    Shabbir