This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
For ADS1294/1296/1298 the ADC resolution changes to 16 Bits at 32khz sampling rate? I want to use ADS1294/ADS1298 for EMG application.
As per data sheet for 32KSPS the ADC OUTPUT IS 24 status bits + 16 bits per channel × 8 channels = 152 bits. Is this correct?
Are you sure with this?? I was reading in the forum that The datasheet info is not correct & the ADC samples are always 24 bit even at maximum sampling rate of 32Khz.
Hi,
You are right -
"The statement on page 53 is a mistake. The data will always be 24 bits in length."
And, there is no 64-kSPS data rates available.
Thanks